990-6401C-001

Connect the Signal Cables in Parallel Systems

  1. Connect the optional parallel cables (E3SOPT002*) between all the UPSs of the parallel system.
    NOTE: See Communication Interfaces for location of parallel ports.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.