990-6401C-001

Recommended Bolts and Cable Lugs

NOTICE
risk of equipment damage
Use only UL approved compression cable lugs.
Failure to follow these instructions can result in equipment damage.
UPS rating 10 kVA 15 kVA 20 kVA 30 kVA 40 kVA
Ground/EGC Cable size (AWG/kcmil) 10 8 8 6 6
Bolt size M6 M6 M6 M8 M6
Cable lug type LCA10-14-L LCA8-14-L LCA8-14-L LCA6-56-L LCA6-56-L
Input/bypass/output Cable size (AWG/kcmil) 8 6 4 1 2/0
Bolt size M6 M8 M8 M8 M10
Cable lug type LCA8-14-L LCA6-56-L LCA4-56-L LCA1-56-E LCA2/0-38-X
Neutral Cable size (AWG/kcmil) 4 3 1/0 2x1/0 2x2/0
Bolt size M6 M8 M8 M10 M10
Cable lug type LCAN4-14-L-01 LCA3-56-L LCA1/0-56-X LCA1/0-56-X LCA2/0-38-X
Battery Cable size (AWG/kcmil) 4/0 4/0 4/0 4/0 4/0
Bolt size M10 M10 M10 M10 M10
Cable lug type LCA4/0-38-X LCA4/0-38-X LCA4/0-38-X LCA4/0-38-X LCA4/0-38-X
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.