990-6401C-001

Remove the UPS from the Pallet

  1. Move the UPS to the final installation area using a forklift or the pallet jack.
  2. Remove the shipping materials and the ramp from the UPS.
  3. Loosen the bolts and remove the shipping brackets.
  4. Remove the bracket from the rear of the UPS. Save for reinstallation.
  5. Place the ramp and fasten it to the pallet with the bolts from the shipping bracket.
  6. Roll the UPS down from the pallet.
  7. Move the UPS to its final location and use a wrench to lower the leveling feet. Ensure that the cabinet is level.
  8. For the 10-30 kVA UPSs reinstall the bracket on the rear side and fasten to the floor.

    Rear View of UPS

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.