990-6401C-001

Heat Dissipation

  10 kVA 15 kVA 20 kVA 30 kVA 40 kVA
Normal mode (W) 700 1050 1400 2100 2800
Battery mode (W) 750 1125 1500 2250 3000
ECO mode (W) 200 300 400 600 800
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.