990-6401C-001

Input Contacts and Output Relays

Dry Contact Interface for External Connections

Terminal Function Diagram
J1-1 Configurable output NC
J1-2 NO
J1-3 COM
J2-1 Configurable input Input
J2-2 GND
J2-3 EPO normally closed EPO NC
J2-4 +24 V
J3-1 External battery breaker trip signal Ext_BB_trip +24 V/200 mA
J3-2 GND
J3-3 External battery status signal Ext_BB_trip +24 V/200 mA
J3-4 GND
J3-5 External battery temperature signal Temp 2
J3-6 Battery temperature sensor 2 GND Temp_COM

Dry Contact Interface for Internal Connections

Terminal Function    
J4-1 Internal battery temperature signal Temp 1
J4-2 Temp_COM
J4-3
External
battery status signal
Input_1
J4-4 +24 V
J4-5 Backfeed trip signal +24 V
J4-6 GND
J5-1 Backfeed trip signal for UIB NC
J5-2 NO
J5-3 COM
J5-4 Backfeed trip signal for SSIB NC
J5-5 NO
J5-6 COM
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.