990-6401C-001

Torque Specifications

UPS rating Bolt Size Torque
10 kVA M6 5.59 Nm (4.12 lb-ft)
M10 15 Nm (11.06 lb-ft)
15 kVA/20 kVA M8 5.59 Nm (4.12 lb-ft)
M10 15 Nm (11.06 lb-ft)
30 kVA M8 12 Nm (8.85 lb-ft)
M10 15 Nm (11.06 lb-ft)
40 kVA M10 15 Nm (11.06 lb-ft)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.