990-6401C-001

Recommended Upstream Protection

CAUTION
HAZARD OF FIRE
  • Connect only to a circuit with the below specifications.
  • Connect to a circuit provided with a 175 A branch circuit overcurrent protection maximum in accordance with the National Electric Code, ANSI/NFPA70, and the Candadian Electrical Code, Part I, C22.1.
Failure to follow these instructions can result in injury or equipment damage.
NOTE: Overcurrent protection is to be provided by others and marked with its function.
NOTE: For IT systems or resistance grounding systems, a 4-pole circuit breaker must be installed.
NOTE: For local directives which require 4-pole circuit breakers: If neutral conductor is expected to carry a high current, due to line-neutral non-linear load, the circuit breaker must be rated according to expected neutral current.
UPS rating Source Breaker rating (lr) Breaker type li (x In) setting
10 kVA Input 45 A BDF36045 400 A fixed
Bypass 35 A BDF36035 400 A fixed
15 kVA Input 70 A BGF36070 640 A fixed
Bypass 60 A BGF36060 640 A fixed
20 kVA Input 90 A BGF36090 1000 A fixed
Bypass 70 A BGF36070 640 A fixed
30 kVA Input 110 A HGF36110C 1250
Bypass 90 A HGF36090C 1250
40 kVA Input 150 A HJF36150C 1250
Bypass 125 A HJF36125C 1250
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.