990-6470C-001

Connect the Power Cables in a 100-120 kVA 3:3 UPS

  1. Ensure that all breakers are in the OFF (open) position.
  2. Open the front door of the UPS.
  3. Remove the indicated covers.
  4. Only for dual mains system: Remove the single mains jumper busbars.
  5. Route the power cables through the bottom of the UPS.
  6. Connect the equipment earthing conductor/PE to the PE busbar.
  7. Connect the input cables (L1, L2, L3), bypass cables (L1, L2, L3, N), output cables (L1, L2, L3, N), and DC cables (DC+, DC-).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?