990-6470C-001

Install the IP31 Kit

The images below show the installation of the IP31 kit on a 100-120 kVA UPS. The procedure is similar for the other UPS models.
  1. Install the provided rods in the top plate of the UPS.
  2. Install the top cover(s) and fasten with the provided washers and nuts.
  3. Install the gutter between two top covers and fasten with the provided screws.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?