990-6470C-001

Overview of Configurations

UIB Unit input disconnect device
SSIB Static switch input disconnect device
MBB Maintenance bypass disconnect device
BB Battery disconnect device
UOB Unit output disconnect device
NOTE: In Schneider Electric literature, 'disconnect device' is used as a generic term covering circuit breakers or switches as their position may vary depending on configuration. Details about the individual configuration are found in the electrical diagram and/or by reading the symbol on the front of each disconnect device.

Overview of Single UPS


3:3 384 VDC UPS

Overview of 1+1 Redundant Parallel System


3:3 384 VDC UPS

Location of Disconnect Devices

Locations of Disconnect Devices on the 3:3 UPSs

10-80 kVA 3:3 384 VDC UPS

100-120 kVA 3:3 384 VDC UPS

160-200 kVA 3:3 384 VDC UPS

 
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?