990-6470C-001

Connect the Signal Cables

  1. Output dry contacts (230 VAC)

  2. External battery temperature input contact (Non-SELV)

  3. BB trip output contact (SELV)

  4. Input dry contacts (SELV)

  5. USB port (SELV)

  6. RS232 port (SELV)

  7. RS485 ports (SELV)

  8. Parallel ports (SELV)

  9. Intelligent slot for SNMP card (SELV)

  1. Ensure that all breakers are in the OFF (open) position.
  2. Remove the indicated cover.

    10-80 kVA 3:3 UPS

    100-200 kVA 3:3 UPS

  3. Route the signal cables through the bottom of the UPS as shown below and fasten the signal cables with cables ties.

    10-80 kVA 3:3 UPS

    100-120 kVA 3:3 UPS

    160-200 kVA 3:3 UPS

  4. Reinstall all covers.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?