990-6470C-001

Overview of Input Contacts and Output Relays

Specifications

  Parameter Typical Maximum
Input Voltage (V) NA 5
Current (mA) NA 15
Output Voltage 24 VDC 230 VAC
Current (A) NA 3
  • Input dry contacts:

    • DI2: Normally Closed (NC) input dry contact for the battery disconnect device on the battery cabinet.

    • DI3: Normally Closed (NC) emergency power off input dry contact. When activated (opened), the UPS shuts down immediately.

    • NTC: Input dry contact for external battery temperature sensor.

    • DI1 and DI4: Configurable input dry contacts.

  • Output dry contacts:

    • BB Trip: The output dry contact provides 24 V supply to the auxiliary switch of the battery disconnect device for trip protection.

    • DO1 to DO5: Configurable output dry contacts.

Fixed Input Dry Contacts

Terminals Function Default Application
DI2 Ext BB contact signal Fixed
DI3 Emergency power off (EPO) Fixed
NTC External battery temperature Fixed

Configurable Input Dry Contacts

The input dry contacts provide active signals and it is not necessary to connect an external power supply to trigger the function.

Terminals Function Default Application
DI1 0: OFF
1: UPS ON
2: UPS OFF
3: Battery fault
4: Genset enable
5: Custom alarm 1
6: Custom alarm 2
7: Disable ECO
8: Force inverter off
0
DI4 0

Fixed Output Dry contacts

NOTICE
RISK OF EQUIPMENT DAMAGE
The battery disconnect device contact drive can provide a maximum of +24 VDC 250 mA to the shunt trip release coil. If the value is exceeded, it can damage the UPS.
Failure to follow these instructions can result in equipment damage.
Terminals Function Default Application
BB TRIP Battery disconnect device trip Fixed

Configurable Output Dry Contacts

NOTE: Maximum 5 A/250 VAC, 3 A/30 VDC must be connected to the output contacts. The recommended cable size is 0.5-1 mm².

The output dry contacts provide two passive statuses: Short and open. The output contacts must be connected to an external power supply to trigger the function.

Terminals Function Default Application
DO1 0: OFF
1: Common alarm
2: Normal operation
3: Battery operation
4: Static bypass
5: Output overload
6: Fan inoperable
7: Battery fault
8: Battery disconnected
9: Batter voltage low
10: Input out of tolerance
11: Bypass out of tolerance
12: EPO activated
13: Maintenance mode
14: Backfeed on input
15: Backfeed on bypass
0
DO2 0
DO3 0
DO4 0
DO5 0
NOTE: For single mains system: Configure one of the output dry contacts for backfeed on input.
For dual mains system: Configure two of the output dry contacts for backfeed on bypass and backfeed on input.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?