990-91111L-031

Läckström

380/400/415 V UPS-system, installation med 4 ledare vid 100 % last

UPS-storlek Läckström
20–50 kW 62 mA
60–100 kW 67 mA
120–150 kW 91 mA
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.