Install the Conduit Box on the Modular Battery Cabinet
Only for installation with remote UPS.
UPS rated for maximum 100 kW: Perform the steps below on modular battery cabinet 1.
UPS rated over 100 kW: Perform the steps below on all the modular battery cabinets with external power cabling.
- Remove the conduit box from the rear of the modular battery cabinet.
- Remove the top or bottom gland plate from the conduit box.
- Drill/punch holes for power cables/conduits in the top or bottom gland plate. Install
conduits (not provided), if applicable.
DANGER
hazard of electric shock, explosion, or arc flashDo not drill or punch holes with the gland plates installed and do not drill or punch holes in close proximity to the cabinet.Failure to follow these instructions will result in death or serious injury. - Reinstall the top or bottom gland plate on the conduit box.
- Install the conduit box on the modular battery cabinet. Note that the conduit box is installed in the reverse position.