Connect the Power Cables for a UPS Rated for Maximum 100 kW
| NOTICE |
|---|
|
Risk of equipment damage
Only connect the DC cables from battery breaker to battery breaker in installations
with a UPS rated for maximum 100 kW. For installations with a UPS rated over 100 kW,
see Connect the Power Cables for a UPS Rated over 100 kW.
Failure to follow these instructions can result in equipment damage.
|
- Connect the preinstalled PE cables (0W50448) between the modular battery cabinets as shown.
- Connect the preinstalled DC cables (0W50425) between the modular battery cabinets as shown. Connect DC- to DC- and connect DC+ to DC+ between the modular battery cabinets.
- For installation with adjacent UPS: Follow the UPS installation manual to connect the PE and DC cables in the UPS.
- For installation with remote UPS:
- Optional: You can remove the right side panel from modular battery cabinet 1 for easier access. Reinstall the side panel after power cabling is completed.
- Disconnect the preinstalled PE cable and DC cables from modular battery cabinet 1. The preinstalled power cables are not long enough for connection to a remote UPS.
- Connect the PE cable and the DC cables (not provided) in modular battery cabinet 1.
- Route the PE and DC cables out through the conduit box and into the UPS power cabling area.
- Follow the UPS installation manual to connect the PE and DC cables in the UPS.