990-6161A-001

Install the Seismic Anchoring (Option)

Use the optional seismic kit GVSOPT016.
  1. For installations with adjacent cabinets: Connect the rear anchoring assemblies with the interconnection plate. Repeat the step for all anchoring assemblies for adjacent cabinets.

    Rear View of Installation with Adjacent Cabinets

  2. Mount the rear anchoring assembly to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear anchors is ø13 mm. Minimum requirement is M12 grade 8.8 hardware.

    Rear View of Installation with Adjacent Cabinets

  3. Remove all the screws and the interconnection plate.

    Rear View of Installation with Adjacent Cabinets

  4. Remove the anchoring brackets.

    Rear View of Installation with Adjacent Cabinets

  5. For installations with adjacent cabinets: Reinstall the interconnection plate.

    Rear View of Installation with Adjacent Cabinets

  6. Remove the two transport brackets and the indicated bolts from the rear of the modular battery cabinet.

    Rear View of the Modular Battery Cabinet

  7. Install the rear anchoring bracket on the modular battery cabinet with the provided M8 bolts.

    Rear View of the Modular Battery Cabinet

  8. Push the modular battery cabinet into position so the rear anchoring bracket connects to the rear anchors. The front anchoring bracket is installed in the final installation steps.

    Rear View of the Modular Battery Cabinet

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.