990-6161A-001

Prepare Modular Battery Cabinet 1 for Signal Cables

Only for installation with remote UPS.

  1. Remove the gland plates and the brush plates from the front of modular battery cabinet 1.
  2. Perform one of the following:
    • For installation without conduits: Reinstall the brush plates.
    • For installation with conduits: Drill a hole in the gland plates for conduits, install conduits, and reinstall the gland plates.

    Modular Battery Cabinet 1 without Conduits

    Modular Battery Cabinet 1 with Conduits

  3. Route the Class 2/SELV signal cable through the right gland/brush plate and into modular battery cabinet 1.
  4. Route the non-Class 2/non-SELV signal cable through the left gland/brush plate and into modular battery cabinet 1.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.