990-6161A-001

Interconnect Modular Battery Cabinet 1 and the Adjacent UPS

Use installation kit 0H-220042 and optional seismic kit GVSOPT016 for this procedure.
  1. Remove the static switch module.
  2. Push the UPS into place. For seismic anchoring, ensure that the rear anchoring bracket connects to the rear anchor.
    1. Lower the front and rear leveling feet with a wrench until they connect with the floor. Note that the UPS must match the height of modular battery cabinet 1. Use a bubble-leveler to check that the UPS is level.
  3. Push modular battery cabinet 1 into place. For seismic anchoring, ensure that the rear anchoring bracket connects to the rear anchor.
    1. Lower the front and rear leveling feet with a wrench until they connect with the floor. Use a bubble-leveler to check that modular battery cabinet 1 is level.
    NOTICE
    Risk of Equipment damage
    Do not move the cabinet after the leveling feet have been lowered.
    Failure to follow these instructions can result in equipment damage.
  4. Only for seismic anchoring: Install the two interconnection brackets between modular battery cabinet 1 and the UPS.

    Modular Battery Cabinet 1 and the UPS

  5. Install the interconnection screws between modular battery cabinet 1 and the UPS.
  6. Install the baying covers in the top and bottom between modular battery cabinet 1 and the UPS.
  7. Reinstall the static switch module.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.