990-5909B-012

Caractéristiques du couple de serrage

Taille de vis Couple
M4 1,7 Nm (1,25 lb-ft/15 lb-in)
M5 2,2 Nm (1,62 lb-ft/19,5 lb-in)
M6 5 Nm (3,69 lb-ft/44,3 lb-in)
M8 17,5 Nm (12,91 lb-ft/154,9 lb-in)
M10 30 Nm (22 lb-ft/194,7 lb-in)
M12 50 Nm (36,87 lb-ft/442,5 lb-in)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Contenu utile ?