990-914302A-001

Final Mechanical Assembly of the Power Cabinets

DANGER
hazard of electric shock, explosion, or arc flash
All panels and covers must be properly reinstalled prior to energizing the UPS.
Failure to follow these instructions will result in death or serious injury.
  1. Reinstall the three plates in the given order (a-c) on each power cabinet.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?