990-914302A-001

Install the Rear Seismic Anchoring for the UPS and the Battery Cabinet(s)

DANGER
hazard of electric shock, explosion, or arc flash
Leave the UPS system and battery cabinets covered while making anchoring holes to prevent dust or other conductive particles from entering the system.
Failure to follow these instructions will result in death or serious injury.
DANGER
hazard of tilting
All rear and front anchoring brackets must be installed.
Failure to follow these instructions will result in death or serious injury.
DANGER
hazard of electric shock, explosion, or arc flash
Leave the UPS system covered while making anchoring holes to prevent dust or other conductive particles from entering the system.
Failure to follow these instructions will result in death or serious injury.
  1. UPS: Use the rear anchoring bracket that was attached to the rear of the I/O cabinet pallet. Fasten the two plates from the installation kit 0H-9101 to the rear anchoring bracket of the I/O cabinet with M8 bolts. Note the direction of the plates.
  2. Place the rear anchoring brackets for the I/O cabinet and the power cabinets in the final installation area.
  3. Interconnect the rear anchoring brackets using the provided screws and bolts.
  4. Mark the hole locations.
  5. Drill anchoring holes according to the national and local requirements.
  6. Mount the rear anchoring brackets to the floor. Bolts are not supplied.
  7. Use a bubble-leveler to ensure that the rear anchoring brackets are level. Use the provided leveling shims if necessary.
  8. Lithium-ion battery cabinet: Mount the rear seismic assembly (4 x 870-50102 and M6 x 16 torx screws from accessory kit 0M-95331 and the rear shipping bracket) to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear seismic bracket is ø14 mm. The minimum requirement is M12 strength grade 8.8 hardware.

    Rear View

  9. In systems with more battery cabinets, interconnect the seismic assemblies with the interconnection plate 870-51172 from the accessory kit 0M-95331.

    Rear View

  10. Remove the indicated screws.

    Rear View

  11. Remove the rear seismic bracket.

    Rear View

  12. Install the rear seismic bracket on the battery cabinet(s).

    Rear View

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?