990-914302A-001

Install the Single Utility/Mains Installation Kit 0H-9161

NOTE: This procedure is only applicable to single utility/mains systems.
  1. Install the single utility/mains installation kit 0H-9161 between the input and bypass busbars. Connect L1 to L1, L2 to L2, and L3 to L3.
    NOTE: Two busbars are required for each connection.

    Front View of the I/O Cabinet

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?