Installation Procedure
- UPS: Follow the receiving and unpacking manual to remove the cabinets from the pallet.
- UPS: Position the Cabinets.
- UPS and Lithium-ion battery cabinets: Install the Rear Seismic Anchoring for the UPS and the Battery Cabinet(s).
- UPS: Prepare the I/O cabinet for power cables. Follow one of the procedures:
- UPS: For single mains systems only: Install the Single Utility/Mains Installation Kit 0H-9161.
- UPS: Connect the Power Cables in a 480 V System.
- UPS: Mount the Front Anchoring Brackets.
- UPS: Route the Signal Cables between the I/O Cabinet and the Power Cabinets.
- UPS: Prepare for External Signal Cables.
- UPS: Connect the Emergency Power Off (EPO).
- UPS: Only for external synchronization: Connect External Synchronization.
- UPS: Connect Equipment to Input Contacts and Output Relays.
- UPS: Connect the Modbus Cables.
- UPS: Final mechanical assembly:
- Lithium-ion battery cabinet: Install the Battery Modules in the Battery Cabinet.
- Lithium-ion battery cabinet: Position and Interconnect the Battery Cabinets.
- Lithium-ion battery cabinet: Install the Front Seismic Anchoring.
- Lithium-ion battery cabinet: Install the Battery Modules in the Battery Cabinet.
- Lithium-ion battery cabinet: Connect the Power Cables.
- Lithium-ion battery cabinet: Route the Signal Cables to the Switchgear, Rack BMS, and System BMS Ports.
DANGER |
|---|
|
hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Startup must only be performed by Schneider Electric.
Failure to follow these instructions will result in death or serious injury.
|
For moving or decommissioning the UPS or the Lithium-ion battery cabinets after installation has been completed, see Decommission or Move the UPS to a New Location or Decommission or Move the Battery Cabinet to a New Location.

DANGER