990-914302A-001

Overview of Communication Interface

  1. TCP/IP

  2. DRY CONTACT ports

  3. SMPS I/O

  4. CAN I/O

  5. RS485

  6. System BMS CAN I/O

  7. DC OUT 1 and DC OUT 2

  8. Reset switch

  9. Start-up button

  10. DC IN 1 and DC IN 2

  11. Status LEDs

  12. CAN bus loop termination resistor switch

  13. CAN 1 port, CAN 2 port

  14. Module

  15. EPO

  16. PSU 1 LED

  17. PSU 2 LED

  18. SG IO 1

  19. SG IO 2

  20. MCCB AUX 1

  21. MCCB AUX 2

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?