Position the Cabinets
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Do not step/walk on top of the cabinets.
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
A minimum of one power cabinet and a maximum of four power
cabinets must be placed on each side of the I/O cabinet.
Failure to follow these instructions will result in death or serious injury.
|
- Install the cover 0M-98993 from the installation kit on the right-most power cabinet.
- Install the interconnection cover 0M-82316 from the installation kit on the left-most power cabinet.
- Remove the side panels from the I/O cabinet and install
them on the left side of the left-most power cabinet and on the right
side of the right-most power cabinet.
WARNINGHazard of arc flash- Do not make mechanical changes to the product (including removal of cabinet parts or drilling/cutting of holes) that are not described in the installation manual.
- Move and install the indicated side panels in all installation types (including parallel installations with no air gap between the frames or in installations where the right-most power cabinet and/or the left-most power cabinet is placed against a wall).
Failure to follow these instructions can result in death, serious injury, or equipment damage. - Remove and dispose of the indicated transport bracket from the left side of the I/O cabinet.
- Remove and dispose of the indicated transport bracket from the right side of the I/O cabinet.
- Remove and dispose of the indicated transport bracket from the right side of the I/O cabinet.
- Remove the two metal plates from the I/O cabinet.
- Push the I/O cabinet into position against the rear anchoring bracket – the I/O cabinet will connect to the conic outcroppings on the rear anchoring bracket.
- Fasten the cabinet to the rear anchoring bracket with the two anchor bolts from the installation kit. Torque to 50 Nm (36.87 lb-ft).
- Push the power cabinets one by one into position against the rear anchoring brackets – the cabinets will connect to the conic outcroppings on the brackets.
- Fasten the cabinets to the rear anchoring brackets by tightening the bolts on the front of the cabinets. Torque to 50 Nm (36.87 lb-ft).
- Lower the two front feet on all cabinets until they connect with the floor – use a bubble-leveler to ensure that the cabinets are level. Use the provided levelling shims if necessary.
- Install the top baying brackets on the top of the cabinets and fasten with the provided screws.
- Remove the three indicated plates in the left side of the I/O cabinet.
- Remove the two indicated plates in the left side of the I/O cabinet.
- Mount the M6 screws from the installation kit from right to left in the four marked locations between the I/O cabinet and the power cabinet placed to the left of the I/O cabinet.
- Mount the M6 screws from the installation kit from right to left to tighten the cabinets together:
- Verify that the right-most power cabinet and the left-most power cabinet for the I/O cabinet has the covers (0M-98993 and 0M-82316) and the side panels installed before continuing.
DANGER







CAUTION