990-914302A-001

Specifications for Lithium-ion Battery Cabinets

Charging power in % of output power 40% at ≤ 80% load, 15% at 100% load
Nominal battery voltage (VDC) at 3.8 V per cell

517

Peak current at voltage (A) 

450

Charge current default rate (CA rate) 

0.7

Maximum continuous charge current rate (CA rate) 

1.0

Float charge voltage (VDC) at 4.2 V per cell

571

End of discharge voltage (VDC) at 3.0 V per cell

408

Nominal float voltage (VDC)

571

Maximum continuous 100% depth of discharge power (kW)

184

Maximum partial depth of discharge power (kW)

231

Short circuit rating value (kA) - Isc, RMS (Isc, MAX)

2.9 (9.0)

NOTE: If the battery temperature is higher than the threshold after a full discharge at maximum continuous discharge power, the UPS may have to reduce the charge current to zero to protect the battery.
NOTE: The battery temperature must return to room temperature ±3 °C (5 °F) before a new discharge at maximum continuous discharge power. If not, the battery breaker may be tripped due to overtemperature protection.
NOTE: The working temperature for the busbars should be no more than
100 ℃ (212 °F).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?