990-914302A-001

Install the Battery Modules in the Battery Cabinet

Type A Battery Module

Type B Battery Module

WARNING
hazard of injury and electric shock
  • Be careful when installing and removing the battery modules (>17 kg).
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Install the battery modules on the shelves from top to bottom.
    NOTE: Pay special attention to the location of type A and type B battery modules.

    Battery Configurations for Battery Cabinets with 17, 16, 13, and 10 Battery Modules

  2. Reinstall the plate in front of the battery shelves.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?