About the Book
Document Scope
This document describes the specifications, installation, operation, and maintenance of the Harmony FT6, which is an HMI (Human Machine Interface) device used in industrial or factory automation systems.
This document is intended for users who design systems, or install and maintain components.
Validity Note
This document is valid for Harmony FT6.
The characteristics of the products described in this document are intended to match the characteristics that are available on www.se.com . As part of our corporate strategy for constant improvement, we may revise the content over time to enhance clarity and accuracy. If you see a difference between the characteristics in this document and the characteristics on www.se.com , consider www.se.com to contain the latest information.
Registered Trademarks
Microsoft® and Windows® are registered trademarks of Microsoft Corporation in the United States and/or other countries.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.
Product names used in this manual may be the registered trademarks owned by the respective proprietors.
Available Languages of this Document
This document is available in these languages:
Related Documents
You can download the manuals related to this product, such as the software manual, from the Schneider Electric download center ( www.se.com/ww/en/download ).
Information on Non-Inclusive or Insensitive Terminology
As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.
Product Related Information
If the equipment is used in a manner not specified by the manufacturer, the protection provided by the equipment may be impaired.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Critical alarm indicators and system functions require independent and redundant protection hardware and/or mechanical interlocks.
When you cycle power, wait at least 10 seconds after it has been turned off. If this product is restarted too quickly, it may not operate correctly.
In the event the screen cannot be properly read, for example, if the backlight is not functioning, it may be difficult or impossible to identify a function. Functions that may present a hazard if not immediately executed, such as a fuel shut-off, must be provided independently of this product. The machine's control system design must take into account the possibility of the backlight no longer functioning and the operator being unable to control the machine or making mistakes in the control of the machine.
WARNING |
|---|
|
LOSS OF CONTROL
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
For additional information, refer to NEMA ICS 1.1 (latest edition), "Safety Guidelines for the Application, Installation, and Maintenance of Solid State Control" and to NEMA ICS 7.1 (latest edition), "Safety Standards for Construction and Guide for Selection, Installation and Operation of Adjustable-Speed Drive Systems" or their equivalent governing your particular location.
WARNING |
|---|
|
UNINTENDED EQUIPMENT OPERATION
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
WARNING |
|---|
|
UNINTENDED EQUIPMENT OPERATION
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The following characteristics are specific to the LCD panel and are considered normal behavior:
-
LCD screen may show unevenness in the brightness of certain images or may appear different when seen from outside the specified viewing angle. Extended shadows, or Crosstalk (like extended shadows) may appear on the LCD screen.
-
LCD screen may contain black or white colored spots (dead pixels) and the color display may seem to change as time elapses.
-
When experiencing vibrations within a certain frequency range and vibration acceleration is above what is acceptable, the LCD screen may partially turn white. Once the vibration condition ends, the whitening of the screen is resolved.
-
When the same image is displayed on the screen for a long period, an afterimage may appear when the image is changed.
-
The panel brightness may decrease when used for a long time in an environment continuously filled with inert gas. To prevent deterioration of panel brightness, regularly ventilate the panel. For more information, please contact customer support.
www.se.com/support
WARNING |
|---|
|
SERIOUS EYE AND SKIN INJURY
The liquid in the LCD panel contains an irritant:
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
| NOTICE |
|---|
|
REDUCTION OF SERVICE LIFE OF PANEL
Change the screen image periodically and try not to display
the same image for a long period of time.
Failure to follow these instructions can result in equipment damage.
|
DANGER
WARNING