EIO0000004893.01

Parts Identification (HMIFT65/66/6750)

NOTE: The figures below show HMIFT6550.

Front

Top

Bottom

Rear

A: Status LED

B: Hook

C: Battery slot

D: Ethernet interface (ETH2)

E: Ethernet interface (ETH1)

F: Serial interface ( RS-422/485) (COM2)

G: Serial interface (RS-232C) (COM1)

H: Power plug connector

I: USB (Type A) interface

J: USB (micro-B) interface

K: Safety alert symbol*1

*1 Identifies the safety messages about the battery in Replacing the Battery.

WARNING
UNINTENDED EQUIPMENT OPERATION
  • Do not connect the product to the computer with the USB (micro-B) cable unless the product is powered by the power cable.
  • Remove the USB (micro-B) cable before communicating with the host controller and other types of equipment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?