System Design
This section describes the system configuration with this product and peripheral equipment.
*1 Refer to Accessories.
*2 For information on how to connect controllers and other types of equipment, refer to the corresponding device driver manual of your screen editing software.
To use this product, transferring
project data from the screen editing software is required. For details
about transfer, refer to the software manual.
When
transferring using the USB (micro-B) interface, connect cables in the following order:
-
Attach the transfer cable to the USB (micro-B) interface of this product.
-
Attach the power cable to this product, then connect the power cable to an external power source.
-
Connect the transfer cable to the computer.
WARNING |
|---|
|
UNINTENDED EQUIPMENT OPERATION
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
WARNING