EIO0000004893.01

How to connect the DC Power Cord

  1. Confirm the power cord is not connected to the power supply.
  2. Check the rated voltage.
  3. Remove the DC power supply connector from this product.
  4. Strip the membrane of the power cord, and twist the wire ends.
  5. Insert each power cord wire into its corresponding hole. Fasten the screws of the DC power supply connector to clamp the wire in place.
    NOTE:
    • The necessary torque is 0.56 N•m (5 lb-in).

    • Do not solder the cable connection.

  6. After inserting all three power cord wires, insert the DC power supply connector into the power connector on this product.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?