Certifications and Standards
The certifications and standards listed
below may include those that are not yet acquired. Please check the
product marking and the following URL for the latest acquisition status.
www.se.com/ww/en/download
Agency Certifications
-
Underwriters Laboratories Inc., UL 61010-2-201 and CSA C22.2 No.61010-2-201, Industrial Control Equipment
-
Underwriters Laboratories Inc., UL 121201 and CSA C22.2 N°213, for Industrial Control Equipment used in Class I, Division 2 Hazardous (Classified) Locations
-
IECEx for use in zone 2 gas /zone 22 dust
-
CCCEx
Compliance Standards
Europe:
CE
-
Directive 2014/30/EU (EMC)
UKCA
-
Regulation SI 2016 No.1091
Hazardous Substances
This product is designed to be compliant with the following environmental regulations, even if the product may not fall directly in the scope of the regulation:
-
RoHS, Directive 2011/65/EU and 2015/863/EU
-
RoHS China, Standard GB/T 26572
-
REACH regulation EC 1907/2006
End of Life (WEEE)
The product contains electronic boards. It must be disposed of in specific treatment channels. The product contains cells and/or storage batteries which must be collected and processed separately when they have run out and at the end of product life (Directive 2012/19/EU).
Refer to Maintenance when extracting cells and batteries from the product. These batteries do not contain a weight percentage of heavy metals over the threshold notified by European Directive 2006/66/EC.