Precautions for Building into an End-use Product
This product is designed for use on flat surfaces of IP66K and IP66F enclosures.
Be aware of the following when building this product into an end-use product:
-
The rear face of this product is not approved as an enclosure. When building this product into an end-use product, be sure to use an enclosure that satisfies standards as the end-use product's overall enclosure.
-
Install this product in an enclosure with mechanical rigidity.
-
This product is not designed for outdoor use. UL certification obtained is for indoor use only.
-
Install and operate this product with its front panel facing outward.
-
The necessary torque is 0.7 N•m (6.2 lb-in).
-
IP66F and IP66K are not part of the UL certification.