Replacing the Battery
This product uses a primary battery for data backup of the internal clock. If the battery is depleted, the clock data will be lost. Use only the replacement battery for this product ( HMIZSBA1).
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
EXPLOSION, FIRE, OR CHEMICAL HAZARD
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
LOSS OF DATA
Failure to follow these instructions can result in equipment damage.
|
-
Insert the battery before reconnecting the power supply. Otherwise, the clock will not work properly.
-
After reconnecting the power supply, set up the clock again. Refer to your screen editing software manual on how to set up the clock.
- Disconnect the power supply from this product.
- Touch the housing or ground connection to discharge any electrostatic charge from your body.
- Place the product face down on a clean, flat, level surface.
- Open the battery slot on the top or bottom of this product.
- Remove the spent battery from the tray by touching the battery from the bottom.
- Put the new battery on the tray in accordance with the polarity markings in the tray and on the battery.
- Insert the tray into the battery slot.
-
Reconnect the power supply to this product.
NOTE: After reconnecting the power supply, set up the clock again. Refer to your screen editing software manual on how to set up the clock.
DANGER
DANGER