7EN02-0421-03

Alarm configuration

You can configure the insulation alarm threshold and delay to suit to the electrical applications you want to monitor.

You can access the device alarm parameters by selecting Menu > Settings > Ins.Alarm.

The alarm parameters are Ins. Alarm and Ins. Al. Delay.

You can set the parameter values for all commissioned or uncommissioned channels

To modify the parameter value, see Parameter modification using the display.

QR code for this page

Was this helpful?