7EN02-0421-03

Product status light indicator

If the Product status light indicator is red, there is an error in the power system or your device.

The error is one of the following cases:

  • Auto test not OK

  • Product error

  • System error

  • No toroid

  • Toroid disconnect

  • Locating signal unavailable

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.