7EN02-0421-03

ION Setup

ION Setup is a device configuration and verification tool.

ION Setup communicates with the device on the network and provides the basic configuration, which can be done via HMI and also advanced configuration, such as firmware upgrade and other features.

See ION Setup for latest version and instruction to install the tool and to add your device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.