7EN02-0421-03

Display

You can set the contrast and backlight and enable screen saver for the display.

You can access the device display parameters by selecting Menu > Settings > Display.

The display parameters and its allowed and default values are as follows:

The following table is profiled. Check for row profiling before making any changes.
Parameter Default value Allowed values
Contrast 50 % 10 % to 100 %
Backlight 100 % 10 % to 100 %
Screen Saver OFF
  • ON

    If you select this value, the display turns OFF after 5 minutes of inactivity. If you press any button or on any fault, the display turns ON.

  • OFF

To modify the parameter value, see Parameter modification using the display.

QR code for this page

Was this helpful?