7EN02-0421-03

Automatic commissioning

  1. At first power up or factory reset, the device displays Detecting Toroid message with a percentage progress bar.
    NOTE: At first power up or factory reset, the device performs automatic commissioning.
    • If toroid is detected, the Commissioning screen displays. This screen shows the status of commissioning. The following table provides the information of the various displays of commissioning grid.

      HMI Display Information
      Commissioned channel 4
      Non-commissioned channel 4
      Commissioned channel 4 with insulation fault
      NOTE: Channel 4 is provided as an example. The displays are applicable for all 12 channels.
      NOTE: If you have connected a toroid which is not one of the recommended toroids, then the device should be manually commissioned. See Manual commissioning. Refer to the Vigilohm catalog for the most up to date listing of compatible toroids.

    • If toroid is not detected, the No toroid message displays. Perform one of the following action:

      • Check if the toroid is properly connected and navigate to Menu > Settings > Commission > Auto. The device performs automatic commissioning.

      • The connected toroid is not one of the recommended toroids. The device should be manually commissioned. See Manual commissioning.

      NOTE: Refer to the Vigilohm catalog for the most up to date listing of compatible toroids.

  2. You can check the wiring of the system. To check, see Checking wiring connection. If you do not want to check, ignore this step and continue to next step.
  3. Press button to exit the commissioning mode.
    NOTE: The device automatically exits commissioning mode after one hour if manual exit is not performed.
    The device displays Summary screen and the clock icon flashes to show that date and time needs to be set.
    NOTE: If you have connected a new toroid or replaced a toroid, navigate to Menu > Settings > Commission > Auto. The device performs automatic commissioning.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.