7EN02-0421-03

Voltage adaptor (V. Adapt)

You can use voltage adapter to monitor ungrounded power system with a rated voltage higher than 480 V AC/DC.

Two values are available for this parameter:

Value Advised Usage
None (Default) Use when the monitored ungrounded power system rated voltage is ≤ 480 V AC/DC.
VA1T Use when the monitored ungrounded power system rated voltage is > 480 V AC/DC and ≤ 1000 V AC/DC.

See Accessories for more information on voltage adaptors.

QR code for this page

Was this helpful?