Parameter modification using the display
For more information about how the menus are structured, see Device menu.
To modify the value of a parameter, follow either of these two methods:
- 
                  Select an item (value plus unit) in a list. 
- 
                  Modify a numerical value, digit by digit and character value. 
For the following parameters, the numerical value can be modified:
- 
                  Date 
- 
                  Time 
- 
                  Password 
- 
                  Modbus address 
- 
                  Toroid turns 
For Channel Name parameter, the character value can be modified.
Selecting a value in a list
To select a
               value in a list, use the up and down menu buttons to scroll through
               the parameter values until you reach the desired value, then press  to confirm the new parameter value.
Modifying a numerical value
The numerical value of a parameter is made up of digits and the one on the far right is selected by default. To modify a numerical value, use the menu buttons as follows:
Modifying a character value
The character value of a parameter is made up of character and the one on the far left is selected by default. To modify a character value, use the menu buttons as follows:
Saving a parameter
After you have confirmed the modified parameter, one of following two actions occur:
- 
                     If the parameter has been saved correctly, the screen displays Saved and then returns to the previous display. 
- 
                     If the parameter has not been saved correctly, the screen displays Error and the editing screen remains active. A value is deemed to be out of range when it is classed as forbidden or when there are several interdependent parameters. 
Canceling an entry
To cancel the current parameter entry, press the Esc button. The previous screen is displayed.