7EN02-0421-03

Information icons

Icons in the information area of the LCD display provide information such as what menu is selected and the insulation alarm status.

The following table is profiled. Check for row profiling before updating any content
Check for IFL12H row profiling
Icon Description
Main menu
  • System resistance (in the absence of an insulation fault)

  • Measurement parameters menu

  • Monitoring menu

  • System impedance

  • System resistance as primary record in Logging page

Fault log menu
Trend menu
Setting parameters menu and submenu
Display language selection menu
Product identification
  • Indication of an insulation alarm

  • Indication of a transient alarm

  • Indication of product status

  • Indication of channel status

Summary
No alarm
Alarm
NOTE: For transient alarms, this icon flashes.
Toroid disconnect
Date/Time parameters menu
Insulation alarm parameters menu
Network parameters menu
I/O configuration parameters menu
Modbus parameters menu
Commission parameters menu
Password parameters menu
Display parameters menu
Reset parameters menu

QR code for this page

Was this helpful?