Hardware overview
A | Alarm relay | |
B | Auxiliary power supply | |
C | Product status LED | |
D | Communication LED | |
E | Menu button | |
F | No alarm LED | |
G | Esc button | |
H | Alarm LED | |
I | 3 contextual menu buttons | |
J |
Label NOTE: Scan
the QR code to view the device documentation: QR code link
|
|
K | RS-485 communication | |
L | 12 toroid connections | |
M | Voltage input | |
N | LCD screen | |
O | Gasket | |
P | Commercial reference and manufacturing data | |
Q |
Specification Label NOTE: Scan the QR code to view the device documentation: QR code link
|
|
R | DIN mounting clip |
Device commercial reference
Model | Commercial reference |
---|---|
IFL12MCN | IMDIFL12MCN |