7EN02-0421-03

Frequency

You can set the rated frequency of the monitored application.

Four values are available for this parameter:

  • 50 Hz (Default)

  • 60 Hz

  • 400 Hz

  • DC

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.