7EN02-0421-03

Modbus register table format

Register tables have the following columns.
Address
The address of the Modbus, in decimal (dec) and hexadecimal (hex) formats.
Register
The register of the Modbus, in decimal (dec) and hexadecimal (hex) formats.
R/W
Read only (R) or read/write (R/W) register.
Unit
The unit in which the information is expressed.
Type
The coding data type.
NOTE: For the Float32 data type, the byte order follows the Big Endian format.
Range
Permitted values for this variable, usually a subset of what the format allows.
Description
Provides information about the register and the values applied.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?