DOCA0110EN-08

Link150 Webpage Description

Home Tab

Webpage for the Home tab displays the following fields:

Field

Description

Device Identification

Lists the following information about Link150 gateway:

  • User Application Name

  • Product Range

  • Product Model

  • Serial Number

  • Firmware Revision

  • Unique Identifier

  • MAC Address

  • IPv4 Address

  • IPv6 Link-local Address

  • Manufacture Date

Device Physical Location

Locates the Link150-XXYYZZ when you turn ON the Identify Device toggle key. The RS485 LED of the selected Link150-XXYYZZ blinks for 15 seconds with 1 s ON and 1 s OFF (test mode.)

Diagnostics Tab

Webpage for the Diagnostics tab contains the following sub tabs:

Diagnostics Sub Tab

Navigation Menu Webpage

Description

Communication

Ethernet

Displays the following Ethernet statistics for troubleshoot network-related issues:

  • Ethernet Global Statistics (Click Reset to restore the values to factory settings.

  • Ethernet Port 1 Statistics

  • Ethernet Port 2 Statistics

IP Network Services

Displays the diagnostic data for Modbus TCP/IP clients connected to the Link150 gateway.

Read Device Registers

Displays register data for devices connected locally to the Link150 gateway.

Serial Port

Displays the diagnostic data for the devices connected to the serial port. Click Reset to restore the values to factory settings.

System

Displays the status of system statistics.

Redundancy

RSTP Bridge

Displays the diagnostic data of RSTP bridge.

RSTP Ports

Displays the diagnostic data of RSTP ports.

Maintenance Tab

The Maintenance tab displays the Firmware Upgrade webpage.

Settings Tab

Webpage for the Settings tab contains the following sub tabs:

Settings Sub Tab

Navigation Menu Webpage

Description

General

Device Identification

Configures the Link150 User Application Name.

Date/Time

Enables the user to manually set the date and time.

Communication

Ethernet Configuration (Dual Port)

Configures the Ethernet ports.

IP Configuration

Configures the IP parameters including IPv4, IPv6, and DNS settings.

Serial Port

Configures serial communication parameters.

Device List

Configures the Modbus devices.

IP Network Services

Enables or disables the IP network services parameters.

Modbus TCP/IP Filtering

Configures the maximum number of Modbus TCP/IP client connections. Configures the IP addresses that can access the Link150 gateway through Modbus TCP/IP.

SNMP

Configures Simple Network Management Protocol (SNMP).

Advanced Ethernet Settings

Configures the advanced Ethernet settings.

Redundancy

RSTP

Displays the diagnostic data of RSTP.

User Management

User Accounts

Manages the existing and newly added user accounts.

Security

Security

Manages the product certificates.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?