0613IB1313-10

Schematics with MasterPact NT/NW and PowerPact P- and R-Frame Circuit Breakers

Description

For more information, refer to the ULP System User Guide.

ULP Connection

All connection configurations require the BCM ULP cord.

When the second RJ45 ULP port is not used, it must be closed with a ULP line termination.

A Circuit breaker BCM ULP cord or RJ45 male/male ULP cord

B ULP line termination