0613IB1313-10

List of BCM ULP Module Commands and Error Codes

List of Commands

The following table lists the available BCM ULP module commands, their corresponding command codes and user profiles. Follow the command execution procedures accordingly Executing a Command.

Command

Command Code

User Profile

Open circuit breaker Open Circuit Breaker

904

Administrator or Operator

Close circuit breaker Close Circuit Breaker

905

Administrator or Operator

Enable/Inhibit close order Enable/Inhibit a Circuit Breaker Close Order

910

Administrator or Operator

Error Codes

In addition to generic error codes Result of the Command, the BCM ULP module commands generate the following error codes returned in register 8021:

Error Code

Description

4759 (0x1297)

Circuit breaker tripped. It must be reset before the command.

4760 (0x1298)

Circuit breaker already closed.

4761 (0x1299)

Circuit breaker already open.

4763 (0x129B)

FDM121 in local control mode. Remote commands not allowed.

4766 (0x129E)

Previous command still in progress.

4767 (0x12A0)

Inhibit close order enabled.

4777 (0x12A9)

Already in the asked state (valid only for enable/inhibit close order).

Any other positive error code means an internal error.