Status
Predefined Alarms Status
The predefined alarms status register indicates the current status of the alarms:
-
alarm bit = 0: alarm is not active.
-
alarm bit = 1: alarm is active.
The following table details the values for each bit of the alarm status registers:
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x1643 |
5700 |
R |
– |
– |
INT16U |
– |
H |
– |
Predefined alarms status |
|
0 |
Predefined alarm 48 |
||||||||
|
1 |
Predefined alarm 49 |
||||||||
|
2 |
Predefined alarm 50 |
||||||||
|
3 |
Predefined alarm 51 |
||||||||
|
4 |
Predefined alarm 52 |
||||||||
|
5 |
Predefined alarm 53 |
||||||||
|
6 |
Predefined alarm 54 |
||||||||
|
7 |
Predefined alarm 55 |
||||||||
|
8 |
Predefined alarm 56 |
||||||||
|
9 |
Predefined alarm 57 |
||||||||
|
10 |
Predefined alarm 58 |
||||||||
|
11 |
Predefined alarm 59 |
||||||||
|
12 |
Predefined alarm 60 |
||||||||
|
13 |
Predefined alarm 61 |
||||||||
|
14 |
Predefined alarm 62 |
||||||||
|
15 |
Predefined alarm 63 |
||||||||
|
0x1644 |
5701 |
R |
– |
– |
INT16U |
– |
H |
– |
Predefined alarms status |
|
0 |
Predefined alarm 32 |
||||||||
|
1 |
Predefined alarm 33 |
||||||||
|
2 |
Predefined alarm 34 |
||||||||
|
3 |
Predefined alarm 35 |
||||||||
|
4 |
Predefined alarm 36 |
||||||||
|
5 |
Predefined alarm 37 |
||||||||
|
6 |
Predefined alarm 38 |
||||||||
|
7 |
Predefined alarm 39 |
||||||||
|
8 |
Predefined alarm 40 |
||||||||
|
9 |
Predefined alarm 41 |
||||||||
|
10 |
Predefined alarm 42 |
||||||||
|
11 |
Predefined alarm 43 |
||||||||
|
12 |
Predefined alarm 44 |
||||||||
|
13 |
Predefined alarm 45 |
||||||||
|
14 |
Predefined alarm 46 |
||||||||
|
15 |
Predefined alarm 47 |
||||||||
|
0x1645 |
5702 |
R |
– |
– |
INT16U |
– |
H |
– |
Predefined alarms status |
|
0 |
Predefined alarm 16 |
||||||||
|
1 |
Predefined alarm 17 |
||||||||
|
2 |
Predefined alarm 18 |
||||||||
|
3 |
Predefined alarm 19 |
||||||||
|
4 |
Predefined alarm 20 |
||||||||
|
5 |
Predefined alarm 21 |
||||||||
|
6 |
Predefined alarm 22 |
||||||||
|
7 |
Predefined alarm 23 |
||||||||
|
8 |
Predefined alarm 24 |
||||||||
|
9 |
Predefined alarm 25 |
||||||||
|
10 |
Predefined alarm 26 |
||||||||
|
11 |
Predefined alarm 27 |
||||||||
|
12 |
Predefined alarm 28 |
||||||||
|
13 |
Predefined alarm 29 |
||||||||
|
14 |
Predefined alarm 30 |
||||||||
|
15 |
Predefined alarm 31 |
||||||||
|
0x1646 |
5703 |
R |
– |
– |
INT16U |
– |
H |
– |
Predefined alarms status |
|
0 |
Predefined alarm 0 |
||||||||
|
1 |
Predefined alarm 1 |
||||||||
|
2 |
Predefined alarm 2 |
||||||||
|
3 |
Predefined alarm 3 |
||||||||
|
4 |
Predefined alarm 4 |
||||||||
|
5 |
Predefined alarm 5 |
||||||||
|
6 |
Predefined alarm 6 |
||||||||
|
7 |
Predefined alarm 7 |
||||||||
|
8 |
Predefined alarm 8 |
||||||||
|
9 |
Predefined alarm 9 |
||||||||
|
10 |
Predefined alarm 10 |
||||||||
|
11 |
Predefined alarm 11 |
||||||||
|
12 |
Predefined alarm 12 |
||||||||
|
13 |
Predefined alarm 13 |
||||||||
|
14 |
Predefined alarm 14 |
||||||||
|
15 |
Predefined alarm 15 |
M2C/M6C Programmable Contacts Status
The M2C/M6C status register indicates the status of the programmable contacts:
-
status bit = 0: the contact is open.
-
status bit = 1: the contact is closed.
The contact statuses are automatically updated, a reset is not possible.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x2298 |
8857 |
R |
– |
– |
INT16U |
– |
E/P/H |
0 |
Contact 1 status |
|
E/P/H |
1 |
Contact 2 status |
|||||||
|
P/H |
2 |
Contact 3 status |
|||||||
|
P/H |
3 |
Contact 4 status |
|||||||
|
P/H |
4 |
Contact 5 status |
|||||||
|
P/H |
5 |
Contact 6 status |
|||||||
|
– |
6–15 |
Reserved |
Protection Status
The following table details the values for each bit of protection pick-up value registers:
-
protection status bit = 0: protection pick-up value is not overrun.
-
protection status bit = 1: protection pick-up value is overrun, even if the time delay has not expired.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x229D |
8862 |
R |
– |
– |
INT16U |
– |
E/P/H |
0 |
Long-time protection status |
|
1–15 |
Reserved |
||||||||
|
0x229E |
8863 |
R |
– |
– |
INT16U |
– |
P/H |
0 |
Current-unbalance status |
|
1 |
Maximum current status on phase A |
||||||||
|
2 |
Maximum current status on phase B |
||||||||
|
3 |
Maximum current status on phase C |
||||||||
|
4 |
Maximum current status on the neutral |
||||||||
|
5 |
Minimum voltage status |
||||||||
|
6 |
Maximum voltage status |
||||||||
|
7 |
Voltage unbalance status |
||||||||
|
8 |
Maximum power status |
||||||||
|
9 |
Reverse power status |
||||||||
|
10 |
Minimum frequency status |
||||||||
|
11 |
Maximum frequency status |
||||||||
|
12 |
Phase rotation status |
||||||||
|
13 |
Load shedding based on current status |
||||||||
|
14 |
Load shedding based on power status |
||||||||
|
15 |
Reserved |
||||||||
|
0x229F |
8864 |
R |
– |
– |
INT16U |
– |
E/P/H |
0 |
Ground-fault alarm status |
|
P/H |
1 |
Earth-leakage alarm status |
|||||||
|
– |
2–15 |
Reserved |