0613IB1313-10

Minimum/Maximum Event Log

General Description

The system stores the events that concern the metering manager (minimum and maximum values for the Real-Time measurements 1000–1136) in the file number 11.

This file is made up of 136 records and each record is made up of eight registers.

This file contains the minimum and maximum values reached by the real-time measurements.

File Header

The following table describes the file header content:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x1C1B

7196

RW

INT16U

H

File status:

0x0000 = file disabled

0xFFFF = file enabled (factory setting)

0x1C1C

7197

R

INT16U

H

Type of file:

11 = minimum/maximum metering event log

0x1C1D

7198

R

1

INT16U

H

Size of a file = 136 records

0x1C1E

7199

R

1

INT16U

H

Size of a record = 8 registers

0x1C1F

7200

R

INT16U

1

H

File filling mode:

1 = disabled if log is full

File Status

The following table describes the file status content:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x1C2B

7212

R

1

INT16U

H

Size of a file = 136 records

0x1C2C

7213

R

1

INT16U

H

Size of a record = 8 registers

0x1C2D

7214

R

1

INT16U

H

0x0000 = file OK

0x000A = record size smaller than expected

0x0014 = record size larger than expected

0x001E = insufficient memory

0x00FA = internal error

0x00FD = corrupted allocation table

0x00FE = configuration zero

0x00FF = invalid configuration

0xFC00 = invalid file number

0xFD00 = invalid record number

0xFE00 = file not supported

0xFF00 = cannot allocate file

0x1C2E

7215

R

1

INT16U

136

H

Number of records in the file = 136 (real-time zone size)

0x1C2F

7216

R

1

INT16U

1

H

Sequence number of first record in the file (the oldest) = 1

0x1C30

7217

R

1

INT16U

20

H

Sequence number of last record in the file (the most recent) = 136

0x1C31– 0x1C33

7218– 7220

R

DATE

H

Date the last file was reset.

Factory setting = 0x8000 0x8000 0x8000

Minimum/Maximum Event Record

The minimum/maximum event log has a fixed number of records and all record has a fixed number of registers:

Record Number

Registers

Type

Description

1

1

INT16U

Last minimum value (register 1300)

2–4

DATE

Date/time of last minimum value

5

INT16U

Last maximum value (register 1600)

6–8

DATE

Date/time of last maximum value

2

1

INT16U

Last minimum value (register 1301)

2–4

DATE

Date/time of last minimum value

5

INT16U

Last maximum value (register 1601)

6–8

DATE

Date/time of last maximum value

3–135

1

INT16U

Last minimum value (register 130x)

2–4

DATE

Date/time of last minimum value

5

INT16U

Last maximum value (register 160x)

6–8

DATE

Date/time of last maximum value

136

1

INT16U

Last minimum value (register 1435)

2–4

DATE

Date/time of last minimum value

5

INT16U

Last maximum value (register 1735)

6–8

DATE

Date/time of last maximum value